Operators of production facilities these days can not afford to do without effective security measures. The SIT deliver turbine projects to customers in the oil and gas industry – an industry that naturally has a high security awareness in general and cyber security is an increasingly significant part of this. They have a security concept but need to make sure that continuously up-to-date and according to the latest standards. Hence, they needed a security assessment.
The solution was an IEC 62443 assessment which is based on the best known security standard for automation environment and included the following details:
Deep
assessment of compliance to IEC 62443 international standard using
Siemens IEC 62443 Assessment
Security
consultants and engineers from Siemens moderating and facilitating the
assessment
Analysis,
risk identification and classification, definition
of risk mitigation measures and
prioritization of actions
A tool to support compliance with industrial security standards and
customer regulations
Recommendations for risk mitigation and continuous optimization of the security concept with the support of recurring IEC
62443 Assessments
Siemens
Industrial Turbomachinery (SIT) is
located in Finspång/Sweden and is developing and
manufacturing industrial gas turbines.
SIT delivers power plants and projects with industrial
gas turbines across the world.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Siemens Industrial Turbomachinery, Sweden - IEC 62443 assessment to detect potential
risks
Siemens Industrial Turbomachinery, Sweden - IEC 62443 assessment to detect potential
risks