Virtual Training
for Plant Operators in Glass Industry
Sustainability
Increasing degrees of automation, new system
functionalities, larger plants, more flexible production
processes – automation projects are becoming more
complex all the time. To bring products to the market
faster while maintaining a high quality level, it is
essential to have integrated engineering workflows
with short changeover and commissioning times. To meet the requirements for operating a plant in the
glass industry, trained personnel is a key aspect to
achieve production targets. However, on-the-job
training while the plant is in operation is difficult,
because various scenarios require fast and efficient
reactions and new operators often do not have the
necessary experience. Even experienced operators may
have to be trained as a result of plant upgrades and
testing of new exception scenarios. Exception
scenarios, in particular, always pose a risk for
personnel, environment or the plant itself and require
the correct measure at just the right time.
Use SIMIT as virtual training environment to ensure
various application options when training plant
operators. Operating personnel can be trained even
before commissioning the plant – with original
operating screens and automation programs. A digital twin is created with the virtual controller, a
controller that was especially developed for virtual
commissioning and operator training. The automation
program can then be simply downloaded to the
emulated automation system in this Software-in-the-Loop configuration. All reproduceable training scenarios are available on call
during ongoing operation. Any situation can be trained
for realistically in the virtual environment without
affecting production or endangering personnel, the
environment or the plant. While SIMIT creates the ideal
basis for protection and transfer of operating know-how. While the controller is simulated with Software-in-theLoop, the SIMIT UNIT is used to simulate the IO devices
connected to the controller (Hardware-in-the-Loop).
This way you can test your automation program with
simulated process IO, even before commissioning.
Use of existing data to create the simulation
Perform virtual commissioning – even without
any hardware
Testing automation applications environment –
before installation in the real plant
Train plant operators – in a safe but realistic
environment
Safe testing of process optimizations and
enhancements
Virtual Training
for Plant Operators in Glass Industry
Trained personnel is a key aspect
of reaching production targets
Virtual Training
for Plant Operators in Glass Industry
Trained personnel is a key aspect
of reaching production targets
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.