A suburban township in the upper Midwest
United States buys their drinking water from a
major municipal water district. The township’s
water distribution system network has four
connections to the larger municipality’s water
transmission main. The municipality has many
wholesale customers and has implemented
contracts with each customer to limit the peak
flows and the time of day in which they may
occur. If a customer exceeds the limit, they are
assessed significant surcharges.
These potential surcharges make it essential
for wholesale customers to manage water
demand prudently. As a result, many
customers invest in solutions to minimize
usage peaks and control what time of day
they occur, including elevated water storage
towers and control valves at each connection
to the transmission main. The major municipal water district owns
and operates “metering pits” with electromagnetic flow meters (magmeters) immediately
upstream of the control valves owned by each
customer. However, as a rule, the signals from
these meters are not made available to any
customers on a real-time basis. Wholesale water
customers are only provided with datalog
summary reports from these meters on a routine
schedule for billing purposes.
Without a method of measuring flow or receiving
timely flow rate data from the water district, the
suburban township had no means of knowing, in
real time, the amount of water they were
drawing from the transmission main. Therefore,
they did not know if or when they were
exceeding the contractual peak flowrate limits
and incurring significant surcharges from the
water district until they were billed.
The township needed to determine the flowrate at each of its four
connections to the transmission main so that they could control
how much was being drawn at each site. They also needed to
know the total flow from the municipality’s transmission main so
that they would not exceed their contractual peak demand.
The control valves were initially installed without flow
meters. The intention was to use valve position and
upstream/downstream (differential) pressure readings to
estimate the flow using the characteristic curve of the valve.
However, this proved to be too complicated and cumbersome
for the township‘s SCADA system to implement effectively.
The local Siemens representative worked with the township and
their engineer to find a solution to measure the flow rate and
totalize the volume of flow at each of the customer’s control valve
sites. The most significant challenge was the piping configuration,
as all of the valves were previously installed without proper
spacing for a flow meter.
The Siemens representative used a Siemens clamp-on ultrasonic
flow meter (SITRANS FS230) to demonstrate the technology to the customer and
prove that it would reliably meet their objectives.
The valve with
the worst piping configuration was selected for the
demonstration, with the assumption that if the flow meter
would work for the worst site, it would work at the other three
sites as well. If the Siemens flow meter did not work for that site,
the township would need to consider alternate and more costly
flow measurement technologies.
Within minutes of arriving on site, the meter was installed and
providing reliable readings. The unit was allowed to log for a
period of three days. After that, the data was retrieved and
compared to the readings from a competitive magmeter in the
municipal water provider’s metering pit. The logger on the
Siemens clamp-on flow meter helped establish and solidify the
confidence of the owner and the engineer that the meter would
work for these applications.
Cost savings:
If the customer had been unable to use the Siemens clamp-on
ultrasonic flow meters, they would have had to excavate and
install a below-grade vault to house a magmeter and associated
isolation and bypass valves, along with conduit and wiring, at
each of the four sites. This would have required cutting the
water pipe and then going through a cumbersome disinfection
process, both of which would have required lengthy permitting
and costly testing. Further, some of the sites had little or no
room to accommodate such modifications. It was estimated that
this work would have totaled over $250,000. In comparison, the
customer ended up spending $25,000 for the clamp-on meters
along with field service to install some conduit from the pipe to
an existing above-grade SCADA panel.
Time savings:
The customer had already made improvements to the
distribution system and installed four new control valves.
However, their construction contracts were closing and they
could not use their water tower until the new flow controls were
added, so time was a critical factor. The customer saved 3-6
months by using the Siemens clamp-on flow meters instead of
having to construct new vaults to house magmeters.
Improved process reliability
Now that the meters are in place, the customer can control how
much water they are taking from the water district at each of the
four locations and ensure that they do not exceed their
contractual peak. In addition, they can now properly manage the
fill and draw of their elevated storage tank to offset peak
demands, as well as during periods of low demand.
Choosing the right instrumentation for produced water treatment systems
Choosing the right instrumentation for produced water treatment systems
Veröffentlichungsjahr: 2020
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.