A municipal water plant in the southeast United States treats and supplies
potable water to a large metropolitan
area. Part of the process requires accurate flow measurement of the water
from individual pumps to the main
distribution system. The flow meters
provide information of the current
output of the individual pumps. The
customer also requires a device that can
signal a reverse (negative) flow in the
event a pump had stopped. This is so
they would know if water was being
forced back through the pump. If water
flows back through the pump in a
reverse direction and an attempt is
made to start the pump during this
reverse flow, it could cause severe
damage to the pump and motor.
The customer had been using insertiontype, hot-tap magnetic flowmeters from
another manufacturer. Due to the placement of the insertion meters (at least
one in a downward flow condition), the
meters were only lasting from 8 to 12
months and then required replacement
at approximately $5000 each.
The local Siemens representative suggested the customer try the SITRANS
FS230 ultrasonic clamp-on meter,
mounting it on the pipe being monitored before or after the pump,
depend-ing on space and piping
configurations. These are 20 to 36 inch
pipes, ductile, and cast iron, and some
are up to 60 years old.
After a successful demonstration, it was confirmed that the Siemens clamp-on meters provide reliable measurements from outside of the pipe. Since the transducers are not in contact with the process, they cannot be damaged with the process flow like the insertiontype meters. The local Siemens representative also took the time to install a meter to provide an online demonstration of the instrument, and collected data during the test to help assure the customer that the flowmeter would perform as stated. The two meters specified were dualpath clamp-on versions due to the pipe sizes and potential liquid flow profile conditions.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.