A local Siemens representative was visiting a construction site for a new water/
wastewater treatment plant in the Southeast United States. Recent growth in the
local housing market near an EPA wetlands area required the installation of a
new package treatment plant. Discharge
permits for this new plant would require
continuous flow monitoring and strict
discharge levels for chlorine residual. The
accuracy and reliability of the level/flow
measurement and chemical feed control
system was critical. The discharge flume
from the wastewater treatment plant
would be approximately 14 meters from
the wetlands buffer zone.
The representative recommended using
the SITRANS Probe LU transmitter as the
primary level device for a Parshall flume
at the plant effluent. This level measurement would be sent to a chart recorder
which would re-transmit the calculated
flow measurement to the metering
pump’s flow-proportional controller. The
flowproportional controller would receive the flow signal and transmit a dosing signal to the hypochlorite metering
pump.
The Siemens Probe LU was a logical
choice for this critical application. The
client was familiar with the accuracy
and reliability of the instrument because of their experience with the
product at many of their other sites.
The Probe LU became the key component of the hypochlorite dosing system. The client’s confidence in Siemens products provided the
opportunity for the representative to
provide a turnkey solution for the entire hypochlorite system. Siemens
track record of success and the support provided through the local representative was critical to the customer’s
decision.
• Sales and support when and where
you need it Sales and support are
available in your area. Our extensive
global network means you get sales
and support when and where you
need it. By using a single supplier with
local support, the customer was able
to have the equipment installed and
Measuring level in
wastewater treatment
effluent flume
siemens.com/level
calibrated, as well as have their operators trained on a complete flow measurement and automatically controlled
chemical feed system
• More dependable measurement
The non-contacting ultrasonic transducer is immune to problems caused by
suspended solids, harsh corrosives,
grease, or silt in the effluent, making
the measurement more dependable • Ease of use
Simple setup and programming with
handheld infrared programmer or via
PC software
• Reliable performance from Sonic Intelligence Field proven echo-processing algorithms guarantee the most reliable
performance available.
Measuring level in
wastewater treatment
effluent flume
SITRANS Probe LU
Measuring level in
wastewater treatment
effluent flume
SITRANS Probe LU
Veröffentlichungsjahr: 2017
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.