Food processor monitors water usage and verifies meter calibration
Using a Siemes SITRANS FM flow system
Food processor monitors water usage and verifies meter calibration
Using a Siemes SITRANS FM flow system
A food processing company in northern California has a small wastewater
treatment plant to treat its wastewater before releasing it back to the local
municipality. The customer needed a
reliable way to monitor its effluent
flow that is accurate and can be accuracy- verified twice a year.
At the request of the customer, the local
Siemens representative installed a SITRANS FM MAG5100W electromagnetic
flow meter that is now being used in the
wastewater plant of this facility. The
flow meter accurately measures the
quantity of water being returned to the
local municipality. The customer is now
being billed based on the volume of
treated effluent. The SITRANS FM MAG5100W sensor
tube is installed in a 4 inch pipe that
occasionally becomes submerged, but
the application of the Siemens Submersible Kit protects the sensor from
water damage. The remotely
mounted transmitter is mounted in a
cabinet so they can easily see the flow
rate and totalizer amounts, and have
easy access to the output terminals.
The flow signal and the totalizer values are recorded and reported to the
city on a weekly basis.
This meter is tested twice a year by the
representative using the Siemens Verificator. The Verificator is a device that
tests all components to ensure that they
are within factory calibration specifications. The fully automated verification only takes 15 minutes to
perform and provides for a Certificate of Verification. This ensures compliance to the city‘s requirements.
Veröffentlichungsjahr: 2019
Sustainability
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.