COMI is an Italian builder of thermoforming machines for different industries, exporting worldwide. As a long-time partner of Siemens PMA, COMI trusts on SIMATIC products and used WinCC Advanced in the previous projects.
Objectives:
Due to the high turnover of staff in their end customers factories (e.g. Electrolux), the learning times to operate on the COMI machines needed to be reduced. As a possible solution they thought of making a self-explanatory, easier to use, UI with an improved UX.
Siemens was chosen because it has always been a reliable technological partner with a long-term winning strategy. The new system consists of WinCC Unified (PC RT 5K, 1000 Logging Tags, Parameter Control) in combination with a powerful Simatic IPC and S7-1500 PLCs.
Thanks to WinCC Unified technology and openess, COMI machines now offer modern User Inteface with a user exprience similar to what young operators are used to from mobile devices. As a consequence, learning time and mistakes by operators are reduced by 10%. Moreover, COMI automated its processes and so increased productivity by 10% and is now able to win new customers and to acccess new market
The project of the Siemens partner (40-factory.com) started with a brand-new UI/UX design made by Figma (figma.com). The final result shared with COMI, consisting of a brand new SVGs library and a template for the screens, was then applied in WinCC Unified. A CWC completed the project to load the machine settings through a JSON file prepared outside WinCC.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.