An innovative and renewable energy supply was to be set up for the new administrative building of RhönEnergie Effizienz + Service GmbH and an adjacent residential and commercial area. The aim was to achieve a sustainable supply at marketable heating prices for the customers in the neighborhood. The contractor aimed for a supply with almost 100% renewable energy.
To work out the optimal supply solution, a feasibility study was prepared as part of the Heat Network Systems 4.0 funding program. The potential analysis of the available sources showed that a nearby wastewater collector can be used as the main energy source. Based on this, a supply system was developed that can provide cooling and heating by means of a wastewater heat exchanger and two brine-to-water heat pumps. The supply system is supported by a biomethane cogeneration plant and a peak load boiler, as well as several PV systems on the building roofs.
Support in the application process for the optimal design of subsidies.
Preparation of a sustainable and long-term viable concept.
Preparation of a detailed report for the funding agency to achieve Module II funding.
Further planning and coordination of the implementation with the general contractor and the planners.
Long-term contact for the customer on all aspects of energy supply.
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Feasibility study heat network systems, Fulda - Germany
Feasibility study heat network systems, Fulda - Germany