The decoiling line was systematically expanded to enable even bigger sheets to be
processed more efficiently. A second straightener was added followed
by a trimmer (edge cutter). As a result of all these additions, the
installation became a collection of AC and DC motors, various controllers that
did not communicate with each other and operations in different places within
the plant. If a component failed, it was hard to find the problem. But the customers require
continuity and Decomecc also operates 7 days a week. So things had to be improved.
The safety requirements
from the machinery directive and the low voltage directive had to be met and performance had to be improved: the number of errors had to be ruled out completely when printing the sheets.
Retrofit
Siemens service experts upgraded the controllers and a number of old DC motors and also introduced
numerous functional and safety upgrades.
Better ergonomics Siemens service experts replaced the various controllers with a single central SIMATIC S7-1500TF
controller which combines all PLC and safety
tasks. As a result, complex
kinematic functions such as synchronization of the various drives, and
integrated safety are controlled centrally. All the cables and motor
drives (SINAMICS S120 for the line drives and adjustment motors and SINAMICS G120 for the auxiliary drives) are also new. 3 of the 39 motors on the line
were still DC motors; these were replaced with AC models (SIMOTICS M and S).
By combining the
existing motors with new drives, it was possible to achieve significant cost savings for Decomecc.
The controllers are
now grouped together in a new electrical room, with space for expansion in the
future. As a result of the
systematic additions, the old cabinets were dotted around the building. The new
electrical room is more efficient and more ergonomic as heat and noise are no
longer being pumped into the building. The space that was gained has also
made it easier to carry out visual inspections along the line. Safety and functional upgrades The current safety requirements from the machinery directive and
the low voltage directive are now met. After a risk analysis, barriers were provided where necessary. Some zones are no longer accessible while others have
been demarcated using light curtains and light screens.
There were also a lot of functional upgrades. The PLC is integrated in level
2/3, i.e. it is connected to the ERP system so that orders are read in automatically. Operators used to have to type in data
manually which meant that there was a risk of them putting in the wrong
dimensions or numbers. Now that reading in is carried out automatically, the
possibility of errors has been ruled out completely.
Decomecc also prints sheets. The text used to be added via a barcode but if the operator
forgot to scan it, the printing was wrong. Now
that data comes directly from the server.
Another
functional upgrade was the electric paper
winder. There is paper between the coils that needs to roll up when you
uncoil the metal. That used to be done
pneumatically but now it is done electrically. This is also controlled by Retrofit for Drive Systems and as a result the paper tears much less frequently.
Energy savings
As
a result of the retrofit, the installation also uses less electricity. This is deemed pretty
important when there are volatile energy prices. An
eco mode was installed. If the installation is not in use for a certain length of time, the components are switched off. The machines consumption used to be 40 kW when it
was not in operation, now it is 1 to 1.5 kW. It also reduces the wear and tear on the machine.
"A retrofit is
cheaper, more ecological and quicker than installing a whole new line.”
Peter Vanschoenwinkel, COO Decomecc
Better
ergonomics.
Higher sustainability as fewer raw materials are required.
Complex kinematic functions such as synchronization of the various
drives, and integrated safety are controlled centrally.
By combining the
existing motors with new drives, Decomecc achieved
significant cost savings.
The new AC motors are now
completely maintenance-free.
Space saving: The controllers are now grouped together in a new electrical room, with space for expansion in the future. The new electrical
room is more efficient and more ergonomic.
Safety requirements
from the machinery directive and the low voltage directive are met energy savings.
Decomecc, a decoiling and metal cutting company, is a high-tech innovative service center offering the full range of metal processing possibilities for aluminium, steel, and stainless steel. From decoiling, cutting-to-length, slitting, and sawing to laser blanking and CNC milling, Decomecc has all expertise in-house and production capabilities on site.
Decomecc, Belgium - Retrofit for Drive Systems improves safety and performance
Decomecc, Belgium - Retrofit for Drive Systems improves safety and performance
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.