The Tirol Kliniken faced the challenge of standardizing and modernizing the integrated management system of their four state hospitals. The goal was to present various technical systems, such as fire alarm technology and access control, on a single, vendor-agnostic platform. Crucial was the ability to grant individualized access rights to enhance security and efficiency, and to prevent operating errors. Further requirements included a future-proof solution with reliable service, as well as a comprehensive video
surveillance system for property protection and patient safety.
Siemens was able to address the challenges faced by Tirol Kliniken with a comprehensive solution. Various technical systems and facilities, such as fire alarm technology, video surveillance, elevator emergency calls, access control, etc., were presented on a unified interface using the installed integrated control system.The Siemens security management system SiControl, specifically designed for critical infrastructure, enabled personalized features. It was designed to assign individual permissions to all employees, ensuring access only to relevant areas. This system optimizes overview, enhances security, and prevents operating errors. The large number of interfaces – over 400 in total – makes SiControl ideally suited for projects like this. Furthermore, 24/7 support is available for any issues, and ongoing updates support the expanded system. In addition to the new integrated control system, Siemens implemented two new video
surveillance systems in the hospitals. One serves for property protection and the other for patient safety; accordingly, the systems are handled separately. Videos recorded for property protection are stored for a defined period, whereas for patient safety, only live images are displayed, for instance, to visualize the occupancy of a waiting area. In total, Siemens placed over 800 cameras in the four hospitals and integrated previously installed devices into the Qognify VMS video
surveillance solution.
Thanks to the deployment of the latest control and video
surveillance technologies and comprehensive support from Siemens, the clinics are optimally prepared for future requirements in the long term. This not only enables convenient control but also offers maximum possibilities for personalized access configuration. The consolidation of various technical systems (fire alarm technology, video surveillance, access control, etc.) onto a central, unified interface at the Innsbruck site ensures significantly more convenient and efficient management of the entire control system. A significant gain for the clinics is the optimized overview and enhanced security, as the system allows for individual permissions, thereby preventing operating errors. Furthermore, the implemented system stands out due to its high flexibility, quality, and future-proofing capabilities. Additionally, the two distinct video
surveillance systems provide the hospitals with tailored and effective solutions for both property protection and patient safety, optimally adapted to their specific requirements.
The Tirol Kliniken are the largest and most diverse healthcare provider in Western Austria. They comprise four state hospitals in Innsbruck, Hall, Hochzirl, and Natters, with a total capacity of more than 2,400 beds. Together with a nursing clinic and a training center, they form the medical backbone of Tyrol. As a comprehensive healthcare network, the Tirol Kliniken are committed to continuously modernizing and securing their infrastructure. As part of these efforts, they commissioned Siemens with a comprehensive modernization of their integrated management system, aiming to standardize the four hospitals and thus pave the way for a secure future.
Advanced technology for healthcare in Tirol Kliniken - Austria
Ensuring maximum future readiness for Tirol Kliniken
Advanced technology for healthcare in Tirol Kliniken - Austria
Ensuring maximum future readiness for Tirol Kliniken
Fertigstellung: 2024
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.