A number of ongoing reliability issues associated to the pumps, motors and gearboxes of the main cooling water system posed a significant risk to the commercial operation of the Marchwood gas-fired combined cycle power plant.The aim was to improve the control and reliability of the gas-fired combined cycle power station.
Marchwood is a 840MW CCGT power station owned by
Marchwood Power Ltd, a 50:50 joint venture between SSE and ESB international.
All of the electricity at the plant is sold under contract to SSE. Marchwood
began operating in December 2009 and is one of the most efficient gas-fired
power stations in the UK.
Installation of three 2.5 MW SINAMICS PERFECT HARMONY GH180 Drives
Installation of three 10-pole 2.1 MW SIMOTICS HV Motors
Removal of the existing motors and gearboxes
Installation and commissioning on-site
Integration into the existing DCS control system
Energy savings of 150,000 pounds per year
CO2 reduction has also been predicted to drop by 2,100 tonnes over the next year, leading to additional cost savings.
IDS-Solution (all from a single source)
<CompanyDescription>Marchwood is a 840MW CCGT power station owned by Marchwood Power Ltd, a 50:50 joint venture between SSE and ESB international. All of the electricity at the plant is sold under contract to SSE. Marchwood began operating in December 2009 and is one of the most efficient gas-fired power stations in the UK.</CompanyDescription>
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Maximum energy savings on Marchwood power plant
Maximum energy savings due to Variable Speed Drive with a SINAMICS PERFECT HARMONY GH180 CONVERTER
Maximum energy savings on Marchwood power plant
Maximum energy savings due to Variable Speed Drive with a SINAMICS PERFECT HARMONY GH180 CONVERTER