The
customer requirements for the replacement were very high. The new converter must
be fail-safe and its related auxiliary systems must not lead to a system
shutdown in case of a failure. To replace the old system there was a limited
downtime of three days. If a non-preventive system shutdown occurs, the hole
drive train must be fixable within 24 hours. These requirements can be met and
even exceeded by the characteristics of the SINAMICS PERFECT HARMONY GH180.
With over 17,000 delivered units worldwide (2019) it is the most established
MV-Converter on the market. Due to redundant cooling fans and a mechanical cell
bypass with automatic neutral-point-shifting, the GH180 ensures trip free
operation.
Combined with a state of the art SIMOTICS HV M Motor, the concept of Siemens
Large Drives Applications (LDA) was coherent but not yet complete. Since it was
impossible to integrate a new converter into the existing operation room before
the deadlines, Siemens engineers had a sophisticated container solution in
mind. Fully installed, pre-tested and pre-mounted at site, the Drive System can
be put in operation during a very short, planned downtime.
In the unlikely event of a transformer
failure, this GH180s transformer cabinet can be replaced quickly through a
removeable container top. Due to the dusty environment a closed cooling system
for the container was desired. This was realized with redundant air-water
exchanges connected to an onside water-cooling system. The outcome is a positive
energy balance compared to electrical AC-cooling. If the primary cooling water
circuit fails, the system automatically switches to an available fountain water
supply.
Siemens Scope of Supply
- VFD Container solution with removeable top,
partly redundant and Air-/Water Heat Exchanger Modules fully installed and
pretested.