Hanson is a
cement production company located in the United Kingdom. It used to be called
Castle Cement before the rebranding in 2009. The concern is part of the HeidelbergCement
Group and currently employs 3,500 people in jobs ranging from specialist and
professional managers through to production operatives. The principal markets
of Hanson are the major contributions in England, Wales and the central belt of
Scotland.
Hanson
Cement takes the environment very seriously. Therefore, the company installed a
12MW solar farm which replaces 2/3 of the burned coal with alternative fuels. In
addition, Hanson was the first UK cement producer to carry out annual
environmental audits of its sites. Furthermore, the Ketton site, is a flagship
plant in working with local conservation groups to protect the biodiversity. Today
it is one of the most efficient cement-factories in Europe. However, the cooler
produced a lot of wasted heat, so Hanson was convinced there is still additional
frame for improvements. This is how Siemens Large Drives Applications (LDA)
came into play.
So far Hanson
Cement and Siemens already been cooperating closely with one another. Therefore,
Hanson invited some engineers to find solutions for an increased energy
efficiency. Together they decided that it would be a good step forward to
install variable speed drives on the cooler. These drives give Hanson the
opportunity to cool down the clinker to variable stages according to the needs
of the plant, which leads to a more energy-efficient production process.
The
SIMOTICS HV M motors which driving the back-filter fans, are controlled by the
SINAMICS PERFECT HAMRONY GH180 drives. Each day over 1000 data points are
captured to the cloud. Through the implementation of SIDRIVE IQ together with
Siemens, Hanson Cement can use the collected data to monitor the drive-train 24/7
and to plan their maintenance intelligently. Due to this data-analytics system,
Siemens is able to offer services such as Expert Assistance and Expert Diagnostics.
Hanson
Cement never imagined that the cooperation with Siemens would have such an
impact on their daily business. Together, problems can be solved before they
arise.
LDA Solutions
at a glance:
Since
Hanson Cement has very restrictive rules about data security a two-way
connection system was no option for them.
Accordingly,
the Siemens Service experts proposed to use SIDRIVE IQ Services as the one-way
communication solution.
Therefore,
all existing equipment was connected to the SIDRIVE IQ platform:
2 x SINAMICS PERFECT HARMONY GH180
and 2 x High-Voltage-Motors at Ketton site
1 x SINAMICS PERFECT HARMONY GH180,
1 x SINAMICS GM150 and 2 x High-Voltage-Motors at Purfleet works
Furthermore,
the customer requires for Siemens to provide an own infrastructure, so a M876
cellular modem was implemented.
As
soon as the assets were connected Hanson Cement was able to benefit from SIDRIVE
IQ Services to a greater amount, since the related digital cloud- and
expert-based services optimized the availability and productivity of their
plant to the fullest extent possible.
By use of Expert Diagnostics,
Siemens service experts continuously monitor the connected components and
inform the customer as soon as they detect anomalies.
Via Expert Assistance, Hanson Cement
gets immediate support in case of an unpredictable motor or converter
breakdown.
Minimized
unplanned downtimes: Optimizing maintenance activities with continuous
condition monitoring
Enhanced
plant availability: Identifying changes in the operating states at an early
stage
Time
and cost savings: Early planning and optimization of maintenance and service
activities
Hanson Cements Ketton-Works is a large cement plant and quarry based in the village of Ketton in the country of Rutland in the United Kingdom. Now owned by HeidelbergCement, the plant produces around one tenth of the United Kingdom´s Portland cement needs. Ketton-Works employs around 220 people and is at the forefront of sustainable cement production, namely through the increasing use of non-fossil fuels for the kilns.
SIDRIVE-IQ
for Hanson Cement´s Ketton and Purfleet plant
SIDRIVE-IQ
for Hanson Cement´s Ketton and Purfleet plant
Fertigstellung: 2018
Kontakt
Kontaktieren Sie unseren Vertrieb für weitere Informationen und um direkt zu besprechen, wie unsere Produkte und Lösungen Ihnen helfen können, Ihr Problem am besten zu lösen.
Verwandte Links
Bitte beachten Sie, dass einige der Links möglicherweise nur im Intranet verfügbar sind.