The NXPLUS C 24 blue GIS is the ideal solution for us, as it is just as compact and low-maintenance as conventional medium-voltage systems, but without the climate-damaging SF6.
Nicolaus Winkelmann, Project Manager for Substations at Hamburger Energienetze GmbH
The NXPLUS C 24 blue GIS, a gas-insulated medium-voltage switchgear from the blue GIS portfolio. Like conventional SF6-insulated systems, it has compact dimensions and is encapsulated from the ambient air. The system uses the insulating medium Clean Air, a mixture of pure components of the ambient air. This technical gas offers excellent insulating properties but has no negative impact when released into the atmosphere.