“Although we are technology independent, we invariably choose Siemens for these types of projects. The Simotics S servomotors and Sinamics S120 drives are not only reliable, but also meet the high dynamic range requirements that a fleece layer requires.”
Retrofit was done in less than 2 weeks time thanks to the experience of the machine builder.
Recognition ensures more agility 
Since the Siemens components are integrated into the TIA Portal platform, they speak the same language and can "recognize" each other. This saves a lot of time, especially during commissioning, compared to manual configuration. Because the drive software is integrated into the controller, the drive does not remain a 'black box' in the event of any incidents. “There is a complete symbiosis from motor shaft to PLC."
In addition, the integration of the drive software into the controller ensures that the drive does not remain a 'black box' in the event of any incidents. 
Also important in this project is the role of the T-CPU controller. This is because it is able to take over complex calculations from the drive, so that the latter becomes even more responsive and accurate. No superfluous luxury, because in the fleece layer, 5 axes must be able to work together very precisely by means of a camming function. 
In addition, the Sinamics S120 has a common DC circuit, which means that the braking energy of the various axes can be recovered. The modular construction ensures that defects can be resolved quickly. 
Future-proof 
Thanks to this intervention, the manufacturer has a highly efficient, future-proof machine that meets all contemporary requirements in the field of digitization. 
The reliable Simotics S servo motors and the Sinamics S120 drives ensure that the high dynamic range requirements of a fleece layer are met. 
Moreover, thanks to the T-CPU and its open and visual communication, the customer can easily adjust and optimize the machine himself. In this way, production is always guaranteed.