For the end user, the most important
issue is the process reliability of his plant, so that when a motor fails, a
replacement motor must be on-site within 3 hours.
Wide variance of motors extending from
0.18 – 250 KW and different explosion types of protection based on the business
model – purchase on demand
Together with partner ASF, Siemens
developed a solution for providing motors and supplying them on demand
The complete range of Siemens
explosion-protected motors up to 250 KW
•Siemens can address the complete
portfolio required
We reliably obtain all of the explosion-protected motors required from a single source.
Bernd Korbach with BASF SE is also responsible for technical drive systems and their procurement in the area of Technical Expertise, Global Engineering Services
Fast
support for non-scheduled failures or downtimes
Maximum 3-hour response time after replacing motors
On-call
service 24/7, 365 days
Very
large motor warehouse with approximately 2000 standard LV motors (explosion
protected motors)
Range
of motors is standardized with motors from one manufacturer (Siemens)
Service
partner in the region with technical know-how and expertise – ASF Südwest