Constellium Singen GmbH commissioned Siemens AG with the delivery, installation and cabling of 2 GEAFOL transformers 2,500 kVA and 11 panels of the SIVACON S8 low-voltage switchgear. One challenge here was the confined space (building 9x4 m) and the roof projection, which made delivery difficult.
There was only one supplier who could meet the requirements (Wirth)
The installation was carried out with a 140 t crane
11 panels SIVACON S8 low-voltage switchgear from Siemens
Transformer station with 2 GEAFOL transformers 2,500 kVA
Complete solution with one contact for all components