The company builds machines for the production of cutting, grinding, resinoid bonded discs and cup wheels. Because of the small space available in the machine several junction boxes had to be installed that needed design work in the office and more installation time. The machines are assembled and tested in the factory before they are disassembled and shipped to the customer.
Davide Maternini SPA uses the decentral SIMATIC periphery ET 200AL and ET 200SP to facilitate their production process and save in cost and time. By using the ET 200AL the engineers are able to save time during the planning and implementation phase of the projects, due to the flexible mounting possibility of the modules, therefore reducing the necessary junction boxes. Additionally the diagnostics provided by the ET 200SP modules and the IO-Link sensors, without any programming necessary, allow for a faster installation and debugging during the commissioning phase on the customer site.
Used Products:
SIMATIC ET 200AL
SIMATIC ET 200SP
S7-300
SINAMICS S120 built-in units
"Using the ET200AL gives us a flexibility on the implementation of the projects that is crucial for us to reduce the development costs of the projects."
Allesandro Amodeo, Head of Engineering Department
Reduce assembly and wiring time by 15% through the flexible mounting possibilities of the ET 200AL directly on the machine
Increase in Availability through the detailed diagnosis of the ET 200SP modules and the information from intelligent IO-Link Sensors
Reduction of the cabinet size through the small footprint of the ET 200SP and the possibility of mounting the ET 200AL outside of the cabinet
Davide Maternini SPA is a medium-sized company in Malnate (Italy) which specializes in building machines and equipment for the production of cutting, grinding, resinoid bonded discs, cup wheels in varying diameters. Their product range consists of: mixing machines, hydraulic and electrical presses from 60 to 5000 Tons and high productivity fully automatic rotary machines from 4 to 12 or more working stations.
Davide Maternini - Production machines for Cutting discs, ET 200AL
Machine construction, Italy
Davide Maternini - Production machines for Cutting discs, ET 200AL
Machine construction, Italy
Completion: 2016
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Related Links
Please note that some of the links may be only available in Intranet.
Davide Maternini - Production machines for Cutting discs, ET 200AL