Tethered Caps: Single-Cable Servos and Integrated Engineering
New efficiency for advanced caps
Tethered Caps: Single-Cable Servos and Integrated Engineering
New efficiency for advanced caps
Machine Building
Eckel & Sohn Maschinenbau GmbH & Co. KG
Gau-Odernheim Germany
As prescribed by the EU from 07/2024
onwards, new closures for single-use plastic packaging, so-called tethered
caps, pose a particular challenge for production system manufacturers. Targeted
quantities of more
than 100,000 per hour can only be achieved with the shortest cycle times during
assembly. Global competition also demands reduced engineering/throughput times,
i.e. shorter delivery times. Added to this is the fallout from the limited
availability of components during the pandemic.
Tethered
caps no longer feasible without servos: During the pandemic, Siemens
ensured the servo drive system delivery performance and created an adapted
drive design at short notice, with an application engineer later supporting the
machine manufacturer on site with fine-tuning of the dynamics. End-to-end
engineering for all components in the TIA Portal was established for the first
time. Core components of the solution are a new "single-cable servo
system" comprising the compact SINAMICS S210 converter and the SIMOTICS
S-1FK2 servo motor, which is geared towards dynamics and precision. The process was distributed over two
interacting
SIMATIC S7-1500TF and T technology CPUs – one for standard and safety tasks on
the basic machine, and one for PROFINET IRT (isochronous real-time)
communication with the servos on the tool heads of the rotary towers. All
functionalities were rapidly implemented.
Tethered caps are no longer feasible without servos – because every
millisecond counts
Jonas Martin, Deputy Operations Manager, Eckel& Sohn Maschinenbau GmbH
The high dynamics and precision of
the single-cable servo drive – in combination with the technology CPUs –
already enables high quantities and product quality. The target for the near
future is over 100,000 tethered caps per hour. End-to-end engineering saves at
least 50% of throughput time in the electrical sector.
Achieve the shortest cycle times and high
quantities when assembling new tethered caps
Reduce engineering/throughput times
Overcome
limited ability to deliver during the pandemic
Related Links
Please note that some of the links may be only available in Intranet.
Reference Video: Efficient Motion Control with SINAMICS S210