Siemens Logo
Siemens References
Siemens Xcelerator: Börger digital substation - Germany

Power Utilities

ENOVA Power GmbH

Bunde Germany

Börger Breddenberg wind farm
Börger,
Germany
Siemens Xcelerator
For the repowering of the Börger wind farm, the existing NXPLUS C medium-voltage switchgear in the substation from 2017 also had to be adapted. The challenge in this project was to keep the shutdown time of the substation as short as possible to avoid significant revenue losses for the wind farm.
  • Delivery, installation, and commissioning of two IoT-enabled NXPLUS C panels 
  • Retrofit of the existing 4 NXPLUS C panels with IoT sensors 
  • Managed services contract including on-call service 
  • Access to Electrification X – Asset Management: an IoT solution for real-time continuous monitoring of the asset health status
Through the repowering, our Börger-Breddenberg wind farm will nearly double its installed capacity and will be able to meet the annual electricity needs of more than 23,000 three-person households. Siemens provided excellent support for this flagship project. The integration went smoothly with minimal interruptions to ongoing operations. Thanks to modern technology and Electrification X – Asset Management, we can now see a significant improvement in operational management and energy administration, and we recognize a clear added value of using digital monitoring solutions.
David Szilagyi, Team Lead Construction Management at ENOVA Power GmbH
ENOVA Power GmbH relies on state-of-the-art IoT-enabled medium-voltage technology and now has a continuous overview of the health status of the medium-voltage switchgear. It is particularly noteworthy that the existing medium-voltage switchgear has also been equipped with sensors, so the existing panels can also be included in the health analysis. The package is rounded off with the managed services contract – the system is continuously monitored by Siemens service technicians, and any anomalies can be addressed immediately. With this cutting-edge technology combined with Electrification X – Asset Management, the highest availability of the substation is ensured, which guarantees maximum availability of the medium-voltage switchgear. Additionally, revenue losses due to substation downtime are minimized.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Contact Sales
ID: 41564