The cullet plant was integrated into the batch-house controller during operation
Environmental aspects
Expand the capacities
First time SIMATIC PCS 7 at Gallo
Glass
It
was sort of like open-heart surgery in which additional controllers were
embedded
SIMATIC
PCS 7
System
redundancy
“Thanks to the integrated solution and the expertise of the batch systems engineering company, the SIMATIC PCS 7 process control system found its way to Gallo Glass.“
Mo Mashinchi, project manager at Gallo Glass
The implemented solution is environmentally sustainable and has given Gallo Glass the desired increase in efficiency and availability.
And thanks to system redundancy, Gallo Glass was also able to expand the capacities.
As an added bonus, the technologies were developed in such a way that it’s theoretically possible to add two more melting furnaces.
Gallo Glass, established in 1958, is a state-of-the-art highly-innovative glass manufacturer based in Modesto/California, specialized in glass packaging for the wine & spirits industry. The recent 18-month upgrade (2017/18) proved to be a complex task: In addition to a cold furnace repair, it involved expanding and integrating the cullet plant, including the belt loading station.
Raise your glasses!
Raise your glasses!
Raise your glasses!
Completion: 2018
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.