The client has a "Hot Stretch Line" with 1 SIMOVERT MASTERDRIVES rectifier and 9 SIMOVERT MASTERDRIVES drives. Because the series is obsolete in 2020, the client wishes to retrofit these drives to SINAMICS S120.
The client has a shutdown of 2 weeks in the summer, so the migration needs to be done in this time frame.
To make the client's mind better, we did the retrofit of 1 inverter during a normal weekend shutdown. With this way the client got confidence in the whole migration.
Siemens service experts delivered, installed and commissioned the new SINAMICS S120 drives (1 BLM; 9 SMM) .
Challenges:
Delivery time of the necessary materials
Executing the installation and the commissioning during the shutdown of 2 weeks
The line regulation is controlled in the S7 PLC above the drives. Some fine tuning of the drive regulations was still needed.
Delivered and executed within a restricted time frame. There were no delays for the restart of the plant because of this project.
Spare part availability.
Free addition of an intervention contract for drives degree A for 1 year.
Glanzstoff-Textilcord, located in Luxembourg, is specialized in the manufacturing of premium textile reinforcements for the Rubber industry by converting handmade fibres like polyester, polyamide, aramid and hybrid in addition to processing rayon yarns. The special know-how of Textilcord Steinford in processing multimaterial fibres as well as specific expertise in interface bonding enables Glanzstoff-Textilcord to supply major well known tire manufacturers worldwide. In addition, Glanzstoff-Textilcord manufactures a wide range of technical fabricates that are used in material rubber goods (MRG) such as hose, flexible structures and airsprings, but also in the composite industry. A workforce of 140 manufactures approximately use 16.000 tons of dipped fabric each year with the state-of-the-Art equipment.
Glanzstoff factory, Belgium - Retrofit of Masterdrives secures spare part availability
Glanzstoff factory, Belgium - Retrofit of Masterdrives secures spare part availability
Completion: 2018
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.