New construction in new territory: Uzbekistan’s first float-glass plant
The real net output ratio for this project was the highest ever for Horn
Glass
New construction in new territory: Uzbekistan’s first float-glass plant
The real net output ratio for this project was the highest ever for Horn
Glass
Glass
Horn Glass Industries AG
Plößberg Germany
Since May 2020, Horn Glass has been equipping the country’s first
float-glass plant on behalf of Zarafshon Oyna LLC. “We’re extremely proud to
be implementing this major project as a turnkey solution,” says Markus Frank,
Deputy Director, Glass Plant Technology at Horn Glass. The medium-sized
enterprise is in charge of planning, delivering, and commissioning all the
technological equipment in the new plant, which will be handed over to the
customer on a turnkey basis in the summer of 2021.
Before the float-glass plant begins delivering its planned daily
capacity of 250 tons, Horn Glass will have provided an impressive scope of
supply, including planning the melting tank, tin bath, and annealing lehr and
delivering all the refractory material, the firing system for natural gas and
diesel oil, batch and cullet chargers, stirrers, coolers, and measuring and
control technology. The company will also supply the tin bath with its
associated technological equipment, which includes a shielding gas mixing
station. These will be accompanied by the entire annealing lehr and
automation system for the hot end. As a Siemens Solution Partner, Horn Glass
once again opted for the Simatic PCS 7 process control system, this time
Version 9.0. The process automation architecture is designed for maximum
flexibility, thanks to a redundant client-server structure. Process
optimization is provided by the powerful Simatic PCS 7 Process Historian
archive and reporting system and a remote VPN service. The plant sections are
integrated in the process structure by three AS 410 single station automation
systems. SCALANCE communication modules and Simatic ET 200 I/O modules are
used in the network. Functional security for the industrial thermoprocessing
technology was implemented using fail-safe Simatic ET 200SP-F I/O modules.
The Simatic PCS 7 process control system with its modular system platform is
ideal for this plant.
Bundled expertise from a single source through the experienced Siemens Solution Partner Horn Glass
Use of state-of-the-art technologies ensure efficiency, productivity, quality
Solutions are scalable for further future investments
Horn Glass is responsible for all the
technological equipment required for the construction of Uzbekistan’s first
float-glass plant. Fully automated production is expected to begin in the
summer of 2021. The real net output ratio for this project was the turnkey
specialist’s highest ever.
Related Links
Please note that some of the links may be only available in Intranet.