In the era of rapid
development of AI, the demand for “computility” has increased sharply in all walks of life. Zhangjiakou, Hebei Province,
is the core city of the Beijing-Tianjin-Hebei hub of the national “East Data, West Computing” project,
where the first single largest data center cluster in China, Hoyinn (Huailai)
Technology Industrial Campus is located. With the rapid
increase of data center load, traditional power distribution is facing new
challenges in terms of capacity, space occupation, energy consumption, delivery
cycle, operation and maintenance, the customer needs an integrated solution to solve the mentioned challenges.
Integrated
power module solution composed of SIVACON low-voltage cabinets from Siemens.
The integrated power module
solution is factory pre-fabricated, which can shorten the project cycle by
about 60% in both installation and commissioning.
Compared with similar products,
the integrated power module is more "compact", with a 30% reduction
in area occupation compared to traditional solutions. The internal power
distribution lines of the module are greatly reduced, leading to lower line
losses and a link efficiency of up to 95.6%, which can effectively help HOYINN Data Center improve its PUE.
The 3WA/3WL intelligent air circuit breaker
built into the SIVACON low-voltage switchgear is a truly IoT-enabled circuit
breaker, fully meeting HOYINN Data Center's requirements for safety, intelligence, and
greenness.