By using the digital twin, we were able to save half of the commissioning time in assembly, so that we could use this time for other commissioning activities.
In cooperation with Siemens and other partners and suppliers, Hugo Beck was able to halve the commissioning time and save up to 30% on packaging material compared to conventional machines. Packaging volume is also reduced by 10%. Using recyclable uncoated paper instead of plastic wrap is another advantage.