Saudi
Arabia is an extremely hot, arid country and water scarcity has been a
challenge for centuries. The most common way to supplement insufficient water
supply is to purify seawater through desalination.
Close to
the city Al Khafji KACST (King Abdulaziz City for Science and Technology) build
the world’s largest solar-powered sea water reverse osmosis (SWRO) desalination
plant. The plant receives power from a neighboring solar power plant with a
connected capacity of 20 megawatts and is designed to produce 60,000 cubic
meters of fresh water per day covering demand of 150,000 people and which can
be further extended to produce 90,000 cubic meters per day. The plant operation
is based on available solar energy, so that the largest possible share of
sustainable energy is used for water production. This not only leads to
significant CO2 savings, but also to lower operating costs.
The
ambitious project was developed and implemented by the water desalination
experts of Rawafid Industrial and Advanced Water Technology (AWT). The engineers
had several compatibility restrictions and little time for planning and construction.
For the
electrical, automation and instrumentation packages, Siemens was chosen as the
general contractor. The team has succeeded in getting all the systems and
components within the required short time to plan, manufacture and deliver.
With the
SINAMICS PERFECT HARMONY GH180 from Siemens Large Drives Applications (LDA) an
energy efficiency of at least 96.5% for the entire drive system is achieved in
all states of operation. Thanks to redundant cooling fans and an advanced cell bypass
the converter has an unrivaled level of reliability. It boasts the predicted
failure rate of less than one per 100,000 hours of operation and is designed to
continue operation even with a 30% input voltage sag. All SINAMICS PERFECT
HARMONY GH180 Drives meet the IEEE519-1992 requirements for voltage and current
harmonic distortion and in this case even exceed the more stringent
requirements for line harmonics of the Saudi Arabian grid code by 75%. Furthermore,
the converter can deal with motor cable lengths up to 2300 meters as standard.
Process
Tolerant Protection Strategy (ProToPS™) process tolerant protection strategy
can give operators enough advance warning to evaluate a drive disturbance and
respond appropriately to avoid a system shutdown. An integrated condition
monitoring extension checks winding temperatures and bearing vibration of the
entire drive train. It triggers an alarm when a threshold is reached and stops
the motor if thresholds are passed.
LDA technology
ensures maximum system availability of around 98 percent. Centralized process
monitoring and automation ensure maximum energy efficiency and sustainable
water supply.
GH180s equipped with cell bypass, redundant
rank of cells and ProToPS
(MTBF >> 100.000h, limited by
blower live time only)
Drives in compliance with Saudi
Arabian Distribution Code (November 2008)
SINAMICS
PERFECT HARMONY GH180 has an energy efficiency of at least 96.5% for the entire
drive system in all states of operation
Predicted
failure rate of less than one per 100,000 hours of operation
Enables
to continue operation even with a 30% input voltage sag
SINAMICS
PERFECT HARMONY GH180 is compatible with any motor type on the market
Smallest
footprint on the market
Simplified
maintenance procedures
In Saudi Arabia freshwater is a precious and rare commodity. At same time, demand of the private sector, the agricultural sector and the industry sector is rising rapidly. To cover this, Saudi Arabia, a country largely composed of desert, has been desalinating seawater for a long time. Concerned about the consequences of climate change, the Saudi Arabian utility KACST is now using the first-time solar power for the energy-intensive process. This is an important step towards providing a sustainable water supply.
Related Links
Please note that some of the links may be only available in Intranet.