Maka Systems GmbH is a supplier of systems in the field of mechanical engineering for CNC special machines in wood, aluminum and plastic processing, as well as model making. The company employs approximately 150 people and is based in Nersingen, Germany. Objectives:
Check the feasibility of the project for the offer at an early stage
Increase in productivity due to less waste
Reduction of the program processing time
Reduction of ramp-up time of the actual machine
Training sessions and intensive support during implementation of the digital twin (DT)
Use of Create MyVirtual Machine and Run MyVirtual Machine for the SINUMERIK ONE
A complete DT with mechanical system, kinematics and signal supply can be created within one week
DT can also be used by end customers
"MAKA Systems GmbH, based in Nersingen, sets course for a digital future with the SINUMERIK ONE and the digital twin from Siemens."
Alexander Hiller - Head of Electrical Design and Application Technology
Executable and usable product for the end customer
Avoidance of waste
Shorter manufacturing times
Start of production immediately after commissioning
The PM270 5-axis moving gantry milling center is used for machining laminated wood and glass-fiber reinforced plastic. The SINUMERIK ONE CNC system was designed in advance as a digital twin using "Create and Run MyVirtual Machine".