To convert the COMOS database structure from the classic cDB database (Classic Data Base) to the current-day iDB database (Industrial Data Base) single-handedly, without involving any Siemens experts.
Aside from a smooth overall process, for the change the two administrators also had to ensure that software's shutdown time was as brief as possible
For plant engineers or general contractors, the
central planning software system is the linchpin of the entire software
environment. For such firms to be successful, it is essential that this system
operates perfectly.
COMOS Life-Cycle-Engineering Solution
Improved updating capabilities.
The use of current modules such as the COMOS MRO (Maintenance, Repair & Overhaul) repair and maintenance management system.
The elimination of the interface for the Excel spreadsheet calculation program, which until that point one had to maintain oneself.
The migration from the cDB to the iDB was seen as an opportunity for cleaning up the database, which had swelled over the years, and optimizing the workflows at the same time.
Since 1925, the Martin firm has been an established name in the field of combustion system and thermal waste treatment plant engineering. The company holds numerous patents for combustion grates, and over the decades, it has evolved into an internationally active plant engineer and manufacturer. In the fourth generation now, the family-operated company can look back on more 450 successful plant projects worldwide