Change in position of the carrier should not take more than 1.3 seconds
MCS as a supplementary axis allows flexible positioning of the carriers
High dynamic response of the machines due to the extremely short change times of the carriers
Simulation of the transport system allows risks and problems to be identified at a preliminary stage
"Change in position of the carrier should not take more than 0.3 seconds.“
Gregory Kyd, Technical Manager, PARO AG
High speed and highly flexible assembly machines
Simulation of the behavior model based on digital twin is instrumental in clarifying project risks at an early stage
Efficient project implementation through simple configuration in a familiar environment
PARO AG in Subingen is a leading partner for automation and robotics
Specializes in high-speed and highly flexible assembly machines and systems
Established in 1986, currently with approximately 50 employees
PARO AG is seeking a solution for high-speed and highly flexible assembly machines and systems which permit extremely short change times for the workpiece carriers