Siemens Xcelerator is an open digital business platform that accelerates digital transformation easier, faster and at scale.
The
customer was looking for a solution to achieve the highest possible production
level and availability. The current production level was to be maintained even
in times of crisis. To achieve these goals, the customer wanted to use a
digitalization solution from a trusted partner.
Senseye
Predictive Maintenance, a cloud-based platform, automatically analyzes the
current and future condition of machinery Senseye
utilizes AI algorithms to identify both immediate and future machine issues,
which allows proactive maintenance to be performed and prevents downtime.
Together with Sachsenmilch,
Siemens' service experts defined the right data points for predicting failure
scenarios and utilized new sensors along with the SIPLUS CMS1200 condition
monitoring system for vibration monitoring.
In
addition, recommendations for data-driven maintenance provided by the
Maintenance Copilot Senseye
were utilized to help the maintenance teams.
“What
we like about this project
is that Siemens has know-how on both the technological and the technical sides
as well as in project management."
Roland Ziepel, Technical Manager, Sachsenmilch Leppersdorf GmbH
Highly available plant operations
with drastically reduced production outages.
Reduced maintenance effort and
prevention of unplanned failures and downtimes.
Significant cost savings in the
lower six figures.
Sachsenmilch Leppersdorf GmbH was founded 30 years ago and processes about 4.6 million liters of milk per day, which corresponds to 170 truck deliveries. Since then, the company has been producing the Sachsenmilch brand, which has now developed into the strongest regional brand in Saxony. Unmistakably due to its pink packaging design, it is also an integral part of shelves and refrigerators beyond the Free State of Saxony.
Sachsenmilch Leppersdorf, Germany - Reduced downtime with Senseye Predictive Maintenance
Sachsenmilch Leppersdorf, Germany - Reduced downtime with Senseye Predictive Maintenance
Sachsenmilch Leppersdorf, Germany - Reduced downtime with Senseye Predictive Maintenance
Completion: 2024
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Related Links
Please note that some of the links may be only available in Intranet.