Siemens Logo
Siemens References
For a secure water supply network – Digital Industries, Switzerland
Späni relies on the WinCC Unified visualization system from Siemens.

Electrical & Electronic (E&E)

Späni Elektro Mechanik AG

Altendorf Switzerland

Späni Elektro-Mechanik AG
Altendorf,
Switzerland
Sustainability
When the control system for the existing water supply network began to show its age, the municipality started looking around for a replacement. The goal of the community of Schübelbach was to achieve better integration of the overall water supply network. Späni Elektro-Mechanik AG was the winner of the call for tenders. They impressed by proposing software that would be customised to the water supply system – and not the other way around. A concern was with the question of scalability, so that the water supply network could expand in future.” 
The new Simatic WinCC Unified web-based visualisation system runs together with a Microsoft SQL database for data archiving on a secure Simatic IPC547 industrial PC. With no installation required, the system is accessible via a browser, at the control centre or using other clients. Extension is possible with the ITP1000 mobile industry PC. The control centre consists of an S7-1500 and ET200SP peripheral modules. The pumping stations and reservoirs run using separate logic and are implemented with an ET200SP. Visualisation and operation of the systems are managed locally using an IPC277E or TP700 panel. 
“WinCC Unified sparked our interest in a web-based visualisation solution, leading us to make contact with Siemens on this topic early on in the project.”
Matthias Bamert, Deputy Managing Director andDeveloper at Späni Elektro-Mechanik AG
The true advantages became quickly apparent, noted Bamert: “Using the web access, it is possible to view and control all the water supply network’s systems via the internet. Except for the server where all the data is processed and visualised in the runtime, no additional hardware is required.” This also helps to simplify maintenance: For example, if the on-call service receives an alarm at night, the person in charge can use a device like a PC or tablet to log into the control system, view the detailed message and respond as required. Since fixing the problem can be delayed until the next day in many cases, this can help staff to avoid nighttime work.