In March 2021, the construction of a modern multifunctional stadium in Hradec Kralovestarted.
The new stadium has a capacity of 9,300 people and meets UEFA Category 4 standards, meaning it meets the criteria for hosting international events. It is one of the
most modern football stadiums in the Czech Republic. The
highlight of the stadium are the lighting poles, which are called lollipops
for their shape.
The end customer: the city of Hradec Kralove
Siemens customer: 4 MaR (provided building automation and control systems)
Installation company: DAHASL (the customer of 4 MaR; delivered all low-current technologies)
The technology-packed stadium relies on Desigo building automation and control system and Desigo CC building management platform. DesigoTM and Desigo CC, as a building management system (BMS) platform,
ensure complete management of all HVAC technologies, including the stadium’s lighting. Of the eighteen control cabinets, four are specially
dedicated to lighting control. Each of these four cabinets is equipped with a PXC3.E16A-200A room automation
station, which controls the lighting on one switch and a quarter of the stands.
The solution also provides the following features:
Heating of the football pitch
Control of chilled water
Control of the heat transfer station
Delivered products:
Building automation controllers Desigo PXC4/PXC5/PXC7 + Desigo CC
PXC3.E72-100A room automation stations integrating 63
RDG200KN units in four control cabintes
Cerberus PRO fire protection system
The comprehensive building management system (BMS/SCADA) provides the customer with reliable data on the entire building operation and helps to monitor, control, and improve facility operations at all levels.