Cutting down probability of error during programming and easier handling of changes
Accurate display output with a great deal of information at once
Mounted on a tool holder system, the printing plates are automatically being processed running through a total of 13 process stations. The plant’s capacity can be maxed out, thus allowing for an unattended run over a certain period of time. This way operation can be maintained in between working shifts. Used Products:
CPU 1515-2 PN
S7-1200
SIMATIC ET 200AL
Comfort Panels
SITOP power supplies
S7-SCL
„In order to meet the automotive branche‘s high requirements, it is important to us to cooperate with reliable suppliers ourselves.”
S. Frank, Project manager
45% time saving at spare part changes. Labelling enables good traceability.
Programming mistakes can be avoided with the help of an array indicated SCL-coding, which can be used on any controller.
The comfort panels‘ high resolution and accurate handling allow for a quick access to requested information via touch command
Suso Sondermaschinenbau GmbH is a german engineering company located in Sulzbach-Rosenberg. Founded in 1994, the company is mainly building special machinery for the processing of metals, ceramics and polymers via 3D-milling, drilling, sanding or blanking.
Machine
to produce plugs for individual wiring
harness. Therefor the printing plates have to produce a lot of different pins.