Siemens Logo
Siemens References
Bright prospects
Control system optimizes the productivity of a hot dip galvanizing plant

Machine Building

thyssenkrupp Steel Europe

thyssenkrupp Steel Europe
Duisburg,
Germany
  • In order to guarantee continuous operation, the automation components in the plant will initially be retained.
  • Use of virtualization in order to become less dependent on operating system cycles.
  • Redundant setup of the control system and access via 27 operator terminals and the intranet.
  • Openness for future modernizations.
  • Modern analyses for plant availability, productivity, energy consumption and quality.
  • Availability of the production data over a long period for reasons of traceability.
  • Low training costs for the operating personnel.
The Hot Dip Galvanizing Plant by thyssenkrupp Steel Europe is about 300 meters long with an annual capacity of about 440,000 metric tons of galvanized sheet steel. The products are mainly destined for the car manufacturing industry. The bottleneck plant has been in continuous 24h operation since 1964, interrupted only by maintenance intervalls. It was not technically feasible to expand the existing visualization solution and faults sometimes occurred, so thyssenkrupp decided on a fundamental modernization and partially new solution which gives the option of expanding the system in the future.
  • For the control system, focus relies on the Simatic WinCC V7 SCADA system – redundant and in a virtual IT infrastructure.
  • focus opted for the Simatic Process Historian – also in a virtual environment – as a central long-term data archive.
  • A Simatic IPC547E industrial PC is used as the engineering station for the control system to allow adaptations to the WinCC project to be carried out and tested independently of productive operation.
  • Industry-standard Simatic Thin Clients are used as the hardware for the majority of the operator stations.
"Projects of this kind that need very complex project management are always a challenge. However, we had very positive experiences here in our collaboration with focus. The project was realized without a hitch."
Joachim Tritschler, retrofit project leader
Having completed the conversion to the new WinCC V7 SCADA system, the first step has been taken toward modernizing the plant in the control field as well.
Thanks to the availability of data in the Process Historian and the connection to the ERP system, detailed long-term analyses are now possible which have already led to optimizations in the plant and raised productivity.
Access to the plant via the network is possible at any time and from any location – a great advantage when the operating personnel have questions for the service technicians and maintenance engineers. It is also possible for focus to connect to the plant at any time and therefore offer immediate support in the event of control system problems. 
In the course of this modernization project, the Hot Dip Galvanizing Plant 2 at thyssenkrupp Steel Europe has reached higher outputs and greater process reliability.
The Hot Dip Galvanizing Plant by thyssenkrupp Steel Europe is about 300 meters long with an annual capacity of about 440,000 metric tons of galvanized sheet steel. The products are mainly destined for the car manufacturing industry. The bottleneck plant has been in continuous 24h operation since 1964, interrupted only by maintenance intervalls. It was not technically feasible to expand the existing visualization solution and faults sometimes occurred, so thyssenkrupp decided on a fundamental modernization and partially new solution which gives the option of expanding the system in the future.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Contact Sales
ID: 38764249D5D34353242ED4229EC554CB