The Altenkirchen district water supply association (WKA) and the Wissen municipal utility (SWW) are expanding their water supply, disposal and gas infrastructures with SIMATIC ET 200SP
Supplying
water to around 100 000 residents
Requirements
for automation and performance of the process control system increase
Need
of solution allowing to remain state-of-the art in the future and successively
expand and seamlessly integrate these expansions into the existing plant
network while it is not jeopardizing the ongoing processes at any time
SIMATIC
ET 200SP controller family
CP
1542SP-1 IRC remote terminal unit in combination with TIA Portal
Data
Point Editor as a central management of process data
Special
telecontrol connection editor in TIA Portal enables convenient connection to an
existing remote control network
New
stations can also be easily added through an automatic route search
Guarantee
of the interaction between the existing STEP 7V5.x environment and the new TIA
Portal
Handling
of larger quantities of data is simplified
Prevention
of errors
Saving
money and time through shorter commissioning
More
straightforward and convenient work environment of TIA Portal
Fast
and low-risk integration in the existing water infrastructure network
Related Links
Please note that some of the links may be only available in Intranet.