The dairy Zott is best known for its brands Sahnejoghurt, Jogobella, Primo, Bayernland Käse, Monte and Zottarella. The customer approached us with the following problem:
Troubleshooting is quite complex, resulting in long disruptions in operation, which leads to costs
Updating of the control system software due to Windows 7 problems is imperative
SISTAR V7.5 helps to increase efficiency with the Replay Mode
The bumpless software update both in the visualization and independently of it in the PCU area is a USP of SISTAR -> No production stop
Virtualization of the project successfully implemented
"With SISTAR, we are now saving a good 50% of the time required for troubleshooting."
Thomas Dahl, Project Manager, Zott SE & Co. KG
Commissioning of the new SISTAR V7.5 version in just a few weeks
50% time saving in error analysis and elimination
Siemens has been successfully supporting Zott for a number of years in the implementation and solution of the upcoming automation challenges
Upgrade of the existing SISTAR V7.0 solution to SISTAR V7.5 and focus on the use of the replay functionality.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.