A typical production environment lasts for several years or even decades. In this time, the IT infrastructure is subject to continual change, new requirements are frequently arising and changes can require extensive costs or set-up times.
Trefz wanted to reduce tool costs and set-up times in their production environment and cooprated with different companies (machine manufacturing, ERP systems, tool setting device and Siemens).
Siemens interacted as part of this project and provided the commissioning of the SINUMERIK Integrate Service, with which machine parks can be connected to higher-level IT systems at the company level. The service solution includes the following details:
Manage
MyTools (MMT) for the tool management of
Siemens´ control system was installed on five DMG machines.
Access
MyData (AMD) for the connection to the
tool setting device for the measurement of tools and for the connection to the
ERP System abas
Reduction
of tool costs by 30%
Reduction of set-up times by 50%
No confusion of tools
thanks to clear labelling
With the new digital tool management the tools are
measured in advance and released
Transparency in the tool inventory
Trefz was founded 1969 in Frauenzimmer. At that time the focus was on the
subcontracting of abrasive parts for the electrical and mechanical engineering
industries. Today the company with 25 employees produces assemblies and
sophisticated precision parts according to customer requirements, precisely,
quickly and economically. Trefz operates in the following industries: mechanical engineering,
electrical industry, vehicle construction, packaging technology and medical
technology.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Trefz manufacturing, Germany - Reduced costs up to 30% with SINUMERIK Integrate Services
Trefz manufacturing, Germany - Reduced costs up to 30% with SINUMERIK Integrate Services