SIPART PS2 digital positioner
used on feedwater valve
A large power producer in the northeast US
has a four unit power generation plant that
operates on demand, based upon bid price
to the area ISO. Plant efficiency and speed of
response is crucial.
The Siemens PS2 digital valve positioner is
being used on a feedwater and startup valve
for Unit #3.
The operations department fills the drum
with the controls in manual mode. Startup
procedures call for the operator to provide
an output to the feedwater valve at a
prescribed level. Repeatability and accuracy
of the valve position in response to the
controller output in “manual mode“ is critical
to the drum fill procedure.
The Siemens PS2 positioner replaces a
competitor‘s analog I/P and a pneumatic
input positioner. The PS2 unit includes a
two-wire, valve position feedback
transmitter to confirm the valve position to
the operator in the control room.
The previous analog I/P and pneumatic
input analog positioner did not provide
repeatable valve positioning with the
controller in “manual.” The operations fill
procedures called for an output to the
valve of 50%. The plant experienced a slow
fill that delayed their tie-in to the grid.
Evaluation of the issue revealed that the
valve was only at approximately 25% of
travel. The existing analog devices in series providing input to the valve position was “drifting” with changes
in temperature and vibration. Recalibration did not solve the
control problem.
The Siemens PS2 digital positioner provides accurate, repeatable
control. This device replaced both the analog I/P and the
pneumatic positioner, simplifying the control circuit and
eliminating the components that were “drifting.” The PS2 unit
also provides positive feedback indication at the control room.
The power producer selected Siemens PS2 positioners based
upon several criteria, including, but not limited to:
A history of using over 35 Siemens PS2 units on other
difficult plant applications, including burner-mounted air
damper drives, attemperator valves, and other applications
Local representative, CKNs “Turn Key” on-site, technical
support including design of replacement mounting hardware,
on-site support for installation, configuration,and support of
plant I&C personnel
Siemens ability to provide a position feedback transmitter
integral to the PS2 positioner
Siemens proven track record for providing over 165 field
transmitters for their Unit #4 DCS upgrade project
SIPART PS2 digital positioner
used on feedwater valve
SIPART PS2 digital positioner
used on feedwater valve
Release year: 2018
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.