Actemium BEA GmbH is a global acting and engineering plant construction company in the field of electrical engineering and automation with headquarters in Germany. They work in various industries i. e. raw material transport as bulk-material due to conveyor systems over 10km at temperatures -20°C to 40°C degrees (-4°F to 104°F). Actemium BEA GmbH has been providing energy-related services along the entire life cycle of electrical facilities for over 100 years. This commitment to performance applies to the production of raw materials and power generation.
Delivery of 14x SINAMICS PERFECT HARMONY GH180 GenV and 14x 6kV SIMOTICS motors, both from Nuremberg, which Actemium BEA integrated in thier container solution to fit to onsite requirements.
Subsequent deliveries of 7x SINAMICS PERFECT HARMONY GH180 and 7 SIMOTICS motors every two years agreed as well as transformers, Medium Voltage switch gears, PLC and Low Voltage motors.
The customer was able to realize this customized solution in the best way. This was possible due to the close cooperation between Engineering, Sales and Service.