FarmDroid is a start up company who has captured the European agriculture industry's interest by providing a solution to a work-force problem which made it difficult to have organic Fresh Produce at an affordable price. The end result is a fully automated robot that increases quality and productivity while been environmentally friendly due to its Solar Panel base energy solution.
Objectives:
Lightwieght field robot for sowing and weeding on faming applications
Firmware update gateway solution
Possibility to have SIL rated controller for legal requirements
Serial communication must be present to interface to other devices
Siemens has assisted the customer in finding a solution that will cover their needs now - but also long term when they up scale their piece count and have to support a fleet of robots running. Basic Panel, S7-1500, S7-1200, CM 1241 communication module, Webserver
We have always been enthusiastic about new technologies. We knew that we need to do better with our sugar and then I saw a Siemens video with a GPS solution. This was the starting point for the FD20.
Jens Warming
A small but powerfull and versatile controller that can handle both field data and control of the robot
Remote troubleshooting and adjustment of parameters via PLC's Webserver
Intuitive operator controls via HMI
Easy deployment of firmware via DH485 for custom PCBs on the robot
Advanced system status troubleshooting via Webinterface.
The FarmDroid FD20 is a startling invention for agriculture; an autonomous lightweight field robot that automates sowing and weed removal on farmland. This means that the soil is grown organic, CO2-neutral and without the risk of causing microstructure damage because of the robot’s low weight.