Siemens Electromotor Plant in Bad Neustadt, NX virtual machine
Machine tools, Germany
Siemens Electromotor Plant in Bad Neustadt, NX virtual machine
Machine Building
Siemens AG Motorenfertigung in Bad Neustadt
Error-free and optimized NC programs must be used in production in order to optimally use the machines.
The NC programs must be commissioned quickly and with as little risk as possible
In case of, for example, capacity bottlenecks or machine breakdown, the NC programs must be quickly transferred onto another machine
New machines must be quickly integrated in the production process. For this, the NC programs must be created and prepared accordingly
Simply inserting NC programs, switching to other
machine tools in the event of bottlenecks, and more than 20% shorter program
runtimes - these are just some of the advantages that the Siemens plant in Bad
Neustadt has achieved with the Run MyVNCK application.
NX virtual machine
We offer the customer a virtual image of his machine
The virtual machine comprises an NX CAM with machine simulation and the virtual NC kernel (VNCK) of the SINUMERIK
Further simulation solutions, which integrate the VNCK, are available
The virtual machine with Run MyVNCK…
… is based on the original SINUMERIK software à Increased safety because the virtual machine has the same behavior as the real machine
… supports offline optimization à Increased machine availability because the real machine performs manufacturing operations, whereas the virtual machine is used to test and optimize NC programs
… simulates the exact process à Increased productivity and enhanced planning through exact calculation of the manufacturing time
Siemens Electromotor Plant in Bad Neustadt
Simulation of an INDEX turning center using the VNCK-based simulation system