Zirl wastewater association is modernizing its wastewater treatment plant infrastructure with telecontrol communication based on SIMATIC ET 200SP
Clean water by means of telecontrol technology
Water
Wastewater association Zirl
Upgrading of remote stations connected redundantly to the control center in order to increase operational reliability
Continued use of existing cabling infrastructure for cost reasons
Water – the natural energy for health and well-being – is a scarce commodity. This makes it all the more important to treat water efficiently and cost-effectively so that it can then be fed back into the water cycle. The wastewater association in Zirl in the Tyrol district uses a modern Simatic ET 200SP control system from Siemens for this purpose.
Connection of the remote stations to the control center using SIMATIC ET 200SP as basis
Communication via communications processor CP 1542SP-1 IRC for SIMATIC ET 200SP Distributed Controller based on the protocol IEC 60870-5-104
Telecontrol communication optimally matched to the process through cyclic or event-driven transmission of data
Space-saving thanks to the compact design of SIMATIC ET 200SP and communications processor CP 1542SP-1 IRC
Significant cost savings, around 20% faster commissioning by using the installed infrastructure
Fast troubleshooting and thus reduction of downtimes thanks to extensive diagnostic options
Efficient control and monitoring via the Internet, as the components in the remote stations are accessed from the central control room in the event of a service call
Wastewater association Zirl in Austria is an association of 14 municipalities in Tyrol, operator of channel/sewer systems and wastewater treatment plants
Modernization of several pumping stations and 50 kilometers of collection systems during ongoing operation with telecontrol communication
Adaptation of the control system of the channel/sewer system and wastewater treatment plant to the most recent advancements in engineering