Kinkele GmbH & Co. KG
is one of Germany's leading contract manufacturers of general mechanical
engineering and, with around 300 employees at its Ochsenfurt site, can cover the entire process
if required – from the manufacturing feasibility studies, to demanding welding
and high-precision CNC machining, to the finished painted product.
To engineer ever larger, heavier, and more valuable workpieces
Compensate for increasing staff shortages
SINUMERIK ONE, SINAMICS drives
Digital twin for virtual project planning and commissioning, as well as
efficient service – including Collision Avoidance
Further development of functionalities: Milling head can be swiveled in 1/100 degree steps in two planes
Efficient pendular working mode thanks to two heavy-duty tables
Integration of further processing steps such as robot welding and options for modern tool management
Consistency with existing SINUMERIK 840D machines
The control system must enable connection to the digitalized future.
Michael Graf, Production Manager Kinkele GmbH & Co. KG
Less programming effort due to easy transfer of 80–90% of the program
components from existing SINUMERIK 840D projects
Short standstill times between shutdown of the old system and start of
production with the new machine
Increased machine productivity and flexibility
More options for advanced process automation – semi-autonomous operation
and modern tool management
Expansion of the product range
Staff shortage
CNC heavy-duty cutting
machines: More performance, same foundation
CNC
milling of large parts with SINUMERIK ONE
CNC heavy-duty cutting
machines: More performance, same foundation
CNC
milling of large parts with SINUMERIK ONE
CNC heavy-duty cutting
machines: More performance, same foundation