Siemens Xcelerator is an open digital business platform that accelerates digital transformation easier, faster and at scale.
Robert Bürkle GmbH is a system specialist for presses and coating technology and a solution provider for the furniture, door, flooring, insulation board and PV industry with headquarters in Freudenstadt. In 2023, the company employs around 450 people. Objectives:
Ambitious project schedule
Development of complex manufacturing operation (loading and stacking units), also including robot technology
Reducing stress on valuable resources in development, testing and commissioning
Virtual commissioning of a new system for producing exterior building panels including stacking by robot
Virtual commissioning using NX-MCD, SIMIT and PLCSimAdvanced for testing of the PLC program and the robot operation
SIMATIC Robot Integrator (SRI) for easy integration of the robot into the PLC program or system
“The schedule for the project was ambitious. The only way to keep the deadlines was with virtual commissioning.”
Jürgen Müller, Head of Mechanical Design Special Projects, Robert Bürkle GmbH
Up to 30 % efficiency gains during software development
Efficient integration of the robot in the stacking unit despite complex motion sequences and a challenging space situation
Commissioning of the physical line with pre-tested and verified solutions saves time as well as material and labor costs
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.