Saint Gobain, India - Improved network stability with Industrial Network Analytics Services
Saint Gobain, India - Improved network stability with Industrial Network Analytics Services
Machine Building
Saint-Gobain S.a.
Courbevoie France
The industrial network is the central nervous system of every automation system. Availability and reliability of network infrastructure is crucial for meeting tough production targets. Networks have to meet high level requirements regarding erection, commissioning and project planning, especially when they have been installed by different vendors. Problems during runtime are often caused in the design phase. A network validation (detailed inspection of all relevant parameters) guarantees the trouble-free operation of Profibus/Profinet networks.
In 2008, a manufacturing system at the plant near Bangalore was installed and commissioned with the help of various vendors. However, for Saint Gobain, this big installation came with its own set of challenges in the networking domain. To achieve network stability, even the network speed was reduced in some areas. Having a failure-free network was still a challenge.
Siemens provided answers to Saint Gobain´s problems with the Profibus Network Validation Service. The service involves thorough on-site check of all relevant parameters by Siemens network experts, which improves the operational security of networks and their components. The network architecture consisted of 7 different networks having 140 slaves.
The validation was conducted in accordance to strict guidelines to ensure a complete check of all possible fault locations.
Followed steps:
Detailed study of all control parameters.
Measuring and archiving fieldbus KPIs (Key Performance Indicators).
Validation report prepared in compliance with ISO 9001.
Validation certificate issued.
Installed additional hardware and softwares to monitor and maintain the KPIs.
Key observations through Profibus network validation were:
Deviations of existing network parameters from Profibus guidelines were identified.
Identified areas where the signal strength was below the minimum recommended values.
Distortion of the signal profile in the network was observed.
Identification of other installation inconsistencies.
Increasing signal strength throughout the network by up to 100%
Improvement of the signal profile and network performance
Taking corrective measures for the network architecture
Meeting the Profibus guidelines and quality management requirements for their Profibus network
Improved network stability, availability and reliability - thereby avoiding production loss due to network failures
Saint Gobain Gyproc India Ltd. - the world's leading manufacturer of ceilings, drywalls and gypsum plasters - a part of the 43 billion Saint-Gobain Group, faced intermittent failures in their Profibus networks, mainly because of inconsistencies in the network planning phase.