Many
of the performed tasks at the EWF are ineffective, since there is no repeat aspect in
production and with up to 2,500 boxes being transported in the production
facility, a lot of time during production is spent on searching. Hence, Electronics Works Fuerth wants to reduce the time searching
for materials.
To accomplish the
customers requirement Siemens provided a solution based on SIMATIC RTLS and
Location Intelligence.
Transponders of the real-time locating system (SIMATIC RTLS) are attached to the objects of interest (boxes)
and within the web-based software expansion Location Intelligence, the transponders are associated with an order.
In case of missing
material, the user of Location Intelligence can simply type in the respective
order ID and the real-time position of the associated transponders are
visualized on the factory layout of the customer.
Time to search for material is reduced to a minimum
Amount of paper used inside the production facility can be reduced, since Location Intelligence can update important order details on the ePaper displays of the Simatic RTLS transponders
The Electronics Works in Fuerth (EWF) is quite a special one.
On the one hand, they are producing products for their own business unit, on
the other hand, however, they also act as
a manufacturing service provider for the entire Siemens organization. For that
reason, the nature of their business is low volume, high mix.
Related Links
Please note that some of the links may be only available in Intranet.
Related Contributions
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Electronics Works Fuerth,
Germany –
Reduced searching times during production with RTLS
Electronics Works Fuerth,
Germany –
Reduced searching times during production with RTLS