A high system availability is important for any factory and a malfunctioning system can cause failures, downtimes and conesquential costs. Aktas was using an outdated WinCC version. Thus, adequate troubleshooting for OC failures was not possible and production losses were caused.
Hence, Aktas needed a solution to update the existing automation software.
Siemens service experts offered a suitable upgrade for the outdated software.
The solution included the following details:
Installation of high-performance industrial PC SIMATIC IPC 647D
Upgrade to automation software WinCC 7.5
Reporting and monitoring of data consumption
Less failures
Minimized production losses
Fast troubleshooting
Aktaş Holding, founded in 1938 and established in Bursa, has an understanding dominated by sustainable development and quality, whereby values are produced and kept alive. Today, Aktaş Holding reached a position operating on 6 continents with its products sold in more than 100 countries and among the major firms of the world in their field also with the contribution of expertise in the field of rubber. Aktaş Holding also develops its activities with its productions specifically for the defence industry in addition to the fields of activity such as transport, automotive, structure and industry.
Related Links
Please note that some of the links may be only available in Intranet.
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.
Aktaş Hava production plant, Turkey - Minimized production losses through SIMATIC WinCC retrofit
Aktaş Hava production plant, Turkey - Minimized production losses through SIMATIC WinCC retrofit
Aktaş Hava production plant, Turkey - Minimized production losses through SIMATIC WinCC retrofit