To create a solution to improve the management of entrances to the closed shops following the Covid-19 emergency.
An intelligent device that
automatically counts people in closed rooms, shops… it is the Siemens LOGO!
Born from an idea of Walter
and Matteo Baldassa of the company of the same name in the middle of the
emergency COVID-19. A smart system to quote the flow of customers within the
company premises, and thus avoiding gatherings, equipped with an electrical
system with radio control that allows, through a traffic light positioned at
the entrance of the activities, to manage accesses from a distance. Siemens has
thus supported Baldassa in the creation of an automatic system: the
"SMART" column. Thanks to LOGO! 8, the intelligent micro controller,
through a pair of photocells installed at the store's entry and exit points, it
is therefore now possible to count the number of people inside the store
itself. In this way LOGO! is able to understand whether the access of a
customer who is in the queue can be enabled or not. If this is the case, the
green light of the column is turned on, if not, the red light is turned on.
Adaptation to the contingent situation; ability to respond to an existing request on the market; new customers interested in the proposed solutions
Walter Matteo Baldassa
Contact
Contact our sales for more information and to discuss directly how our products and solutions could help you to best solve your problem.