More in-house goods
transports need to be carried out with less staff. Machine power should replace manpower. No large structural
investments in the infrastructure should be made. The vehicles need to meet the
high hygienic requirements of the healthcare sector.
Sirius Act pushbuttons and indicator lights from Siemens that are available in IP69K degree of protection meet the existing requirement for IP67 degree of protection. They fulfill most stringent hygiene requirements. The modern pushbuttons and indicator lights are technically and visually state of the art.
Users place a high value on optics, haptics and ergonomics, which Sirius Act delivers in all respects.
Andreas Neubert, Sales Engineer at Bleichert Automation GmbH & Co. KG
More goods can be transported in the future without major effort.
Compact technology ensures rationalization in goods transport.
Siemens, as the general contractor, plans the internal transport of goods on a "turnkey" basis.