A growing demand, along with an extended range of available ingredients called for automation of the mixing process
Producing larger quantities in less time regardless of mixture variants
Precise and fast weighing
“The advantage of this automated solution is that we can produce significantly larger quantities in much less time, something which was difficult for us previously, especially with larger orders. Now large orders are not a problem for us any more, regardless of the mixture variants we produce.”
Philipp Kraiss, Geschäftsführer von mymuesli
Usage of Siemens weighing technology für precise weighing
All dosing stations are equipped with a Simatic S7-200 microcontroller as CPU as well as a Siwarex MS (microscale) weighing module and a five-kilogram load cell for the platform scales
Compact weighing units provides immediate data access to the current weight in the Simatic controller without additional interfaces
Simatic S7-200 microcontroller as CPU as well as a Siwarex MS (microscale) weighing module and the five-kilogram load cell enable high-precision weighing results
Final weight of the ordered mixture is measured and documented by legal-for-trade platform scales
Mymuesli, online supplier for individually mixed muesli
566 quadrillion possible muesli combinations
The loss-in-weight application required for the mixing process had to be individually designed and built
Mix it up
Related Links
Please note that some of the links may be only available in Intranet.